Can machine safety enable increased productivity?

Written by

Omron Industrial Automation is a leading manufacturer of technologically advanced industrial automation products and application expertise.

In this third of a series of articles looking at the challenges surrounding machine building, Dan Rossek and Richard Wilkins of Omron examine how safety can be an enabler for increased productivity and reduced total cost of ownership.

There are few issues in machine design that are more emotively loaded than safety, and it is a subject that becomes increasingly complex with every passing year. Not only is it perceived as impacting negatively on productivity, but requirements are becoming ever more stringent and the numbers of people affected are increasing. Previously the safety of the operator during normal production was the primary – if not the sole – focus of the machine safety system; however, it is now equally important to consider those tasked with maintaining, upgrading and repairing the machine throughout its entire life-cycle. In short, safety now has a major impact on the total cost of ownership of the machine.

Traditional machine development project

A traditional machine development project might start with the mechanical design, move on to the control systems design, and finish with the safety system. Some of the safety technologies employed might be more sophisticated, but conceptually this approach has moved forward very little from a complete isolation of the entire power source of the machine. This can often cause problems of its own such as introducing new hazards to the machine, no longer having the capability of monitoring the moving parts of the machine, unnecessary loss of production time or increased wastage. But competition on an increasingly global scale has driven end user requirements for machines that minimise cycle times and reduce downtime. Both of these factors impact on safety; but is it possible to have a safe machine that operators can interact with more closely, or that engineers can repair or maintain perhaps without requiring a complete shut down and lengthy start up? With traditional approaches to safety, the answer is frequently ‘no’, and this is often where incentives to defeat the safety system arise. A new safety standard – ISO 14119 – addresses this very issue. It is not yet a harmonised standard, but it has been through a final draft and will be voted on shortly. It specifies principles for the design and selection of interlocking devices associated with guards, and covers the parts of guards which actuate interlocking devices. In particular, it provides measures to minimise defeating of interlocking devices in a reasonably foreseeable manner, which is important when you consider that, in the event of an accident, it is likely to be all parties involved who will be investigated, including the machine builder, the end user company and the injured individual. Indeed, it is not inconceivable that all three could end up being prosecuted over a given incident.

Traditional approach to safety system design is wrong

So why is the traditional approach to safety system design wrong? When you start with the mechanical system design, then move to the control system design, and only then look at developing the safety system in accordance with your risk assessment to conform with the Machinery Directive, then while you will most likely end up with a safe machine, you almost certainly won’t end up with an optimised machine. We’re not saying that safety is an afterthought in this process, but it certainly isn’t always an integral part of the design, and so it can do nothing to address user requirements for increased productivity, increased flexibility, improved OEE (overall equipment effectiveness) and reduced TCO (total cost of ownership). The problem arises because often safety is a specialist function within the machine design team. But if machine builders can take a multi-disciplinary approach to safety, and make it integral to all aspects of the build, then there are huge opportunities to develop not only better safety systems, but also safety systems which are readily scalable from one machine to another – improving the design and exceeding user expectations while actually reducing development time and costs. In the improved approach, you are doing a much better job of designing out the risk as you go along, which can mean that the required safeguarding can be a much more elegant system. The machine can be more efficient and give greater flexibility. Operators can interact with it more confidently and more closely, potentially giving huge reductions in cycle times. Rather than stopping the entire machine to clear a jam, it may be assessed that it would be more appropriate to isolate the hazards in the particular zone where the blockage has occurred, allowing the operator to rectify the problem safely without halting the entire production line.

Consider safety right from the beginning of the design

Considering safety right from the very beginning of the machine design project also helps to clarify thinking of what level of safety technology might be required. If only a few safety functions are needed, control built around a few safety relays may well be the most appropriate solution. For a greater number of safety functions, a standalone safety controller might provide the best option. Where the application involves a large machine or a complete production line, a safety PLC that looks and feels more like a conventional control product and which integrates more closely with the wider control system will probably be the best solution, offering the greatest number of safety functions through near-unlimited safety I/O.

Safety as an integral part of the machine automation platform

Omron offers control solutions at all levels of safety requirement, but in particular takes an innovative approach to safety in more sophisticated systems by making safety an integral part of the machine automation platform. The Sysmac platform integrates a safety solution within the ‘one connection, one software’ concept. One connection is realised through the use of the Functional Safety over EtherCAT (FSoE) protocol, while ‘one software’ is achieved using Sysmac Studio for configuration, programming and maintenance – the same software that is also used for the motion, logic, vision and robotics aspects of the machine design. Omron’s NX safety system consists of a safety controller and safety I/O units. Both the safety controller and safety I/O can be freely distributed in an I/O rack throughout the network, mixing them in any combination with standard NX I/O. The concept has many advantages. Firstly, it is of great help in integrating the safety design process with the rest of the machine development, rather than having it be the final stage. It also saves programming time and effort, and reduces configuration time, since you don’t have to spend time finding and mapping tags as you might when integrating a conventional safety system with the wider control system. And you end up with a design that is readily scalable to different levels of an automation project. Most importantly, an integrated approach to safety such as this gives designers far greater freedom to address the questions which will impact on machine flexibility and user productivity: does the machine always need to be completely isolated to facilitate user interaction? Does the machine need to stop at all to enable a simple repair? Can the safety system contribute to improved OEE and reduced TCO? And does it remove functional restrictions while actually increasing safety? By moving away from the conventional approach to safety system design, and taking a multi-disciplinary approach right from the very start of the machine development processes, machine builders can tick all of these boxes, whilst reducing costs and development time, and potentially realising a massive competitive advantage.

This article has been published in the November issue of  the Industrial Technology Magazine

Written by
Omron Europe

Omron Industrial Automation is a leading manufacturer of technologically advanced industrial automation products and application expertise. From its European headquarters in Hoofddorp, near Amsterdam in the Netherlands, she operates locally in every European country and is dedicated to providing unrivaled automation products and customized expert solutions for any industry.

The product portfolio includes state of the art Factory Automation services & Know-How, Sensors and Safety, Mechatronics and Drives, Industrial Components and Vision Systems.